What you can do is use the Trigger input to synchronize the modules that are connected in parallel. Note that the settings of each module must be programmed individually. You can also connect the modules in a master/slave configuration using analog programming so that the slave modules follow the master.
Note that you can only parallel load modules with identical voltage ratings.
Both methods are also available when paralleling multiple mainframes.
Applies to: N3300A, N3301A, N3302A, N3303A, N3304A, N3305A, N3306A, N3307A
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |